/content/honeywellbt/us/en/search.html
    title
    subtitle
    Important: testing notification with start and end duration for everone
    Important: testing notification with start and end duration for auth users

    Online shoppers are hungry for selection and speed. They want a strip mall worth of products at their fingertips, ready for delivery by their next meal. In fact, a recent survey shows that 87 percent of online shoppers identified shipping speed as a crucial factor in whether they were going to shop with a brand again, and 47 percent of those surveyed said they would pay more money to get same-day delivery. 

    The high volumes of smaller, individual orders flooding out of warehouses as a result of these e-commerce trends has spurred changes throughout distribution networks that have real consequences for material handling systems. For example, as carriers and shippers look to make the most efficient use of available delivery capacity, automated equipment must handle a wide range of packaging types - such as polybags.

    How do I prepare for polybags?

    To cut costs that come with dimensional weight pricing, more companies are using polybags or envelopes to ship individual e-commerce orders. For many omnichannel distribution centers, this means handling a variety of packaging types - polybags, corrugated boxes, totes - in one operating space. 

    Polybags, with their tendency to bunch up on themselves, bring a unique set of handling challenges. They need to move along a conveyor system with minimal contact and catchpoints to avoid jams and keep product moving. Motor driven roller (MDR) conveyor is the conveyor system of choice.

    What are the advantages of MDR?

    With the growing pressure to quickly ship items ranging in size from pill bottles to bed frames, the material handling industry is facing new challenges. To keep up with e-commerce order fulfillment, ask yourself: Are my conveyors ready for e-commerce? If you're using conventional conveyor systems designed to handle only cases or totes, the answer is probably no.

    No matter the order size or packaging type, effective e-commerce order fulfillment requires moving high volumes of items through distribution processes quickly and efficiently - without damage. Zero-contact MDR technology enables individually-powered zones to instantly stop, maximizing product control, eliminating back pressure and reducing the risk of product damage. 

    This technology maximizes the amount of items on the conveyor, allowing operations to make the most of available space and optimize accumulation density. For e-commerce operations challenged to house an ever-expanding inventory, efficient use of space is critical, ultimately resulting in more orders fulfilled, greater customer satisfaction and a growing business. 

    MDR systems also use fewer conveyor parts, helping lower maintenance requirements and reducing the risk of downtime. Its modular design can scale as operational demand dictates and easily adapt to existing layouts and footprints for easy installation, along with providing the flexibility to change configurations as business needs (and online shopping patterns) shift. 

    But that's only part of the MDR story

    The versatility of MDR conveyor means it is not just limited to e-commerce order fulfillment and polybag handling. An array of advanced features such as a full width belt, an array eye and more can take operations to the next level - to say nothing of MDR conveyor's essential role as part of sophisticated automated material handling solutions. Keep an eye out for these aspects and more in part two and three of Intelligrated's MDR conveyor blog series. 

    In the meantime, read the Intelligrated white paper, Selecting the Right Accumulation Conveyor, for more information on making the right conveyor choice

    To subscribe to our blog and receive exclusive communications and updates from Honeywell Intelligrated, click here.