/content/honeywellbt/us/en/search.html
    title
    subtitle
    Important: testing notification with start and end duration for everone
    Important: testing notification with start and end duration for auth users

    The data center industry is having a moment. Increased demand to collect and process data driven by changing consumer habits and changing business needs means the sector is projected to continue its fast-paced growth. From online shopping and remote work to cloud-based applications and generative AI, data centers help enable the global economy and cultural shifts.

    Along with rapid acceleration, the industry is facing increased scrutiny from regulators, investors and customers to drive down their carbon footprint and reduce energy consumption.

    How data center operators strategize to meet these demands can mean the difference between success and failure. So, holistic, strategic planning – and adaptability – are musts.    

    A holistic approch from the ground up

    Data centers use a lot of energy. For perspective, the largest facilities can consume as much power as a city of a million people.  Data centers as a whole contribute around nearly 1% of green house gas emissions , making it critical for the sector to drive down its energy consumption. It’s not just about the daily operations of a data center that impacts the ability to reach energy and carbon reduction goals – it’s the entire lifecycle of the facility from location identification, construction, operations and decommissioning.

    Reducing the environmental impact of data centers starts with construction, baking in best practices from the drafting table. This includes choosing the optimum location for a new data center development to the reduction of embedded carbon in building materials and intelligent sourcing. 

    It also means identifying reliable, affordable and more environmentally power sources that can keep up with the industry’s 24/7 operations. Data centers need to think about both the IT and OT operations and deploying smart building management strategies and controls can help achieve power usage effectiveness (PUE) targets.

    When it comes to decommissioning a site, data center operators need to have a plan for how they can help to reuse, refurbish and recycle equipment to further support sustainability efforts. Using refurbished or used equipment in a facility’s operations isn’t just kinder to the environment, it can also potentially be a cost-effective approach. 

    As data center planning takes place, it’s essential for different perspectives to be considered in the process, including that of the chief sustainability officer. This practice is becoming more common in the industry today. 

    Managing challenges through an intergrated soltuion 

    With such rapid growth in the industry, data centers are also facing the need to do more with less. Today, the industry is experiencing a need for more qualified employees to address growing operational and reporting requirements. The good thing is that the tools needed to help fill this gap already exist.

    A building management solution can offer data center managers an integrated approach that enables them to digitalize, aggregate and analyze data from OT and IT subsystems, helping create greater efficiencies in facilities without increasing headcount.

    Honeywell offers an end-to-end solution to cover all of your needs 

    At Honeywell, our experts are available to help with end-to-end data center lifecycle planning and maintenance so that customers can focus on more strategic initiatives that can help drive business growth. Our suite of solutions feature tools that can help optimize uptime, improve resiliency, support sustainability and increase efficiency as well as support safety and security efforts. Connect with one of our experts today to learn more about our data center solutions.

     


    [i] Yale, Energy Hogs: Can World’s Huge Data Centers Be Made More Efficient, Fred Pearce, [Accessed June 29, 2023], April 2028


    [ii] Tech Target, Assess the Environmental Impact of Data Centers, Jacob Roundy, [Accessed Aug. 28. 2023], July 2023


    Contact Us

    ­
    ­