/content/honeywellbt/us/en/search.html
    title
    subtitle
    Important: testing notification with start and end duration for everone
    Important: testing notification with start and end duration for auth users

    As the demand for liquefied natural gas (LNG) increases, Honeywell is working with ADNOC to expand production capabilities in the Middle East.

    ADNOC, the state-owned oil company of the United Arab Emirates, will use Honeywell’s LNG technology and equipment at its Ruwais LNG project. The facility is expected to produce up to 9.6 million tonnes of LNG per year. Natural gas is often considered a bridge fuel in the energy transition, providing a lower-emissions alternative to other fossil fuels.

    Honeywell’s natural gas liquefaction equipment, including a coil wound main cryogenic heat exchanger and pre-cooled mixed refrigerant process technology, will be used with electric drive (e-drive) technology to produce LNG at ADNOC’s Ruwais LNG project. The facility will consist of two all-electric liquefaction (e-LNG) trains and be the first in the Middle East and North Africa to run on renewable and nuclear power.

    “LNG is an emissions-reducing and economically viable solution that enables even the most remote locations around the world to use natural gas for energy,” said John Palamara, general manager, Honeywell LNG. “This project highlights our long, trusted relationship with ADNOC and shared commitment to helping enable the energy transition.”

    Honeywell will supply the technology to ADNOC through Technip Energies, which formed a joint venture with JGC Holdings and NMDC Energy for the engineering, procurement and construction of the Ruwais LNG project. Honeywell will also provide technical advisory services during construction and performance testing.

    Honeywell recently acquired Air Products’ Liquified Natural Gas Process Technology and Equipment Business as part of an effort to expand its energy transition technology portfolio and offer customers an end-to-end natural gas solution. Air Products’ proprietary LNG technology has been used for more than 50 years and currently operates in 20 countries around the world. Air Products has supplied key equipment, technology and services to ADNOC since the 1970s.

    To learn more about Honeywell’s LNG technology visit https://uop.honeywell.com/en/industry-solutions/gas-processing/lng/liquefaction-of-natural-gas.