/content/honeywellbt/us/en/search.html
    title
    subtitle
    Important: testing notification with start and end duration for everone
    Important: testing notification with start and end duration for auth users

    In high-volume manufacturing and logistics, palletizers are essential for maintaining smooth operations. However, neglecting their maintenance can lead to significant performance issues. We'll look at the common issues with maintaining palletizers and how they affect your distribution systems and warehouses.

    1. Loss of Time

      When a palletizer is down, the entire production line can come to a halt. The longer the downtime, the greater the impact on production. Common failures like jams or software glitches can cause delays of 15-30 minutes, while more complex issues like motor failure can result in several hours of downtime.

    2. Lost Productivity

      Downtime results in a direct loss of units that would have been palletized. Palletizer failures can also cause bottlenecks in upstream or downstream processes, further affecting overall production line efficiency.

    3. Maintenance and Repair Costs

      Poor maintenance often leads to increased repair costs. Immediate fixes may involve significant labor costs, replacement parts, and specialized technicians. For example, a maintenance visit may cost between $500 to $1,500, and replacement parts can range from $100s to several thousand dollars. Frequent breakdowns can escalate these costs significantly.

    4. Customer Delays

      Palletizer failures can lead to delayed shipments, resulting in penalties, lost contracts, and customer dissatisfaction. Companies may face reputational damage, affecting future orders and long-term customer relationships. For instance, failure to meet delivery deadlines due to equipment failure could result in fines or the need for expedited shipping, adding unexpected costs.

    5. Labor and Operator Costs

      Increased labor costs are another pitfall of poor palletizer maintenance. Operators may need to work overtime to fix issues or meet production targets, increasing labor costs. Additionally, operators may be idle during downtime, leading to wasted labor time.

    6. Overall System Efficiency

      Poor palletizer maintenance affects Overall Equipment Effectiveness (OEE), a key metric for measuring manufacturing productivity. Palletizer failures reduce OEE, leading to significant productivity losses.

    7. Programs to Optimize Repair Costs

      Palletizer overhaul programs are designed to minimize unscheduled repair costs by providing regular maintenance and proactive monitoring. This approach ensures equipment remains reliable and efficient, reducing the likelihood of unexpected expenses and downtime. Additionally, these programs enable budgeting for overhauls and upgrades over time for effective operational expenditure planning.

     

    Conclusion:

    The cost of palletizer failures can vary greatly depending on the scale of production and the frequency of breakdowns. However, it's clear that these failures lead to significant losses in time, productivity, and, ultimately, revenue. Regular maintenance, proactive monitoring, and quick resolution of issues can help minimize these impacts and keep productivity at optimal levels.

     

    Our Solution:

    To avoid these pitfalls, consider the Honeywell Intelligrated Alvey Palletizer Overhaul Program. This program offers:

    Category
    Efficiency Optimization
    Bottleneck Elimination
    Reliability and Uptime
    Maintenance Budgeting
    Annual Assessments
    Semi-Annual Preventive Maintenance Checks
    OEM Parts Inventory
    Dedicated Project Manager

    Join us in optimizing your operations and ensuring the longevity of your equipment with the Honeywell Intelligrated Palletizer Overhaul Program. For more information or to schedule a consultation, CLICK HERE.

    To subscribe to the Honeywell Intelligrated blog and receive exclusive communications and updates, click here.